Part Number: BQ24195L
I developed it using the BQ24195L.
I want to get 5 ~ 5.1V from the PMID pin.
But without input to VBUS I can't got 5 ~ 5.1V voltage.
--- common ---
Battery volt = about 3.7
PMID Cap = 10+10+0.1uF
----------------------
if VBUS apply 5V , PMID = about 5.1V
if VBUS don't apply 5V , PMID = about 3.5V
I always want 5.1V output form PMID Pin.