Part Number: BQ25121
Other Parts Discussed in Thread: BQ25120A, ,
I know this part is being deprecated and that BQ25120a should be used as a replacement where possible, but a first run of devices of our product shipped before the notice and replacement part became available.
A couple devices in our first run came back to us with an issue of drawing too much power at all times, on the order of 100uA to 300uA. After investigation, we found that the current would disappear if we shut off the LDO powering just one sensor on the board (LS/LSO pin). We cut the trace and confirmed that the excess current draw persists (or gets even worse) when we turn on the LDO output and there is nothing connected to the output.
It may be possible that this is a solder issue under the BGA but it's impossible for me to test that. Therefore I'd like to know if behavior like this has been observed before in the field or in the lab, and if my application might be doing anything to trigger the condition. Note that the majority of the devices in this product delivery don't exhibit this behavior and have quiescent currents in line with the datasheet specification, so this would have to either be a part to part variation or just that I've set something to a knife's edge of compatibility. The circuit is based off of the typical application circuit from the datasheet, but with a 10uF cap on PMID, no diode/connection between PMID and PG, and no battery monitoring. Both SYSOUT and the LDO are set to 3.3V in our application.
It's important to me to have this answered because I need to know if this can also happen with the BQ25120a and if there's something I can to do prevent it.
Regards, Nate