Part Number: BQ24773
Hello,
Our current requirement is 10A in which charging current of battery is 4A and system current is 6A. In this case temperature rise of various components is given below.
2. High side MOSFET : 78C
3. Low side MOSFET : 60C
4. Power Path FET : 65C
We have also kept inductor away from the board just to ensure that other components are not heating an inductor. But in this case also, temperature of inductor is going upto 80C. As per the inductor datasheet there will be 40C temperature rise in inductor at rated Irms which is 12A. So what would be the reason behind this temperature rise in Inductos? Please suggest possible solution.
Note: Experiment is done at ambient 25C.
Waiting for your response.
Regards,
Mihir