This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Provide the boost up circuit: 12VDC to 230VAC



We have a device with The specifications of device is 300 Watts 230 V 50 Hz AC , 1.5 Amp We are developing power pack for this device also. It is having a compressor means it will require pure sine wave... So we have selected a 12 V or 24 V (optional) 35 Amp Lion battery.. Please provide the boost up circuit for that from 12 V DC to 230 V AC 50 HZ 1.5 A

We are using the Lion batteries because of the these batteries are light weight, but Lion are explosive. So according to this please provide solutions. (Devices are Medical devices)