Part Number: BQ24773
Hello TI Experts,
Now I am using BQ24773 for 4cells
when no battery connected, external voltage is 24V, system output voltage is only 6V (without load), But the datasheet said the MinSystemVoltage is 9.216V ~
under this condition,I measure REGN 4.5V, acdet above 0.6V,
I disable the auto wakeup,the REGN still 4.5V~
when battery connected,it's normal ,REGN is 5.4V
Sorry that I have asked it in January,but still cann't solve it~
Looking forward for your reply~~Thank you~