Part Number: BQ24031-Q1
Other Parts Discussed in Thread: BQ24031, BQ25100, BQ25120A, BQ24075-Q1
TLI-1520.pdfHi Bill,
Thanks for the clarification on 5V input. Just to confirm, the minimum AC before the device will shift power from the input to the backup battery is < 4.35V?
Regarding the battery, This is a Tadiran TLI-1520 battery. I have a datasheet for the battery (attached) . Will the TPS24031-Q1 be suitable for the charging mechanisms of this battery? The max charge current of the battery is 25mA.
Best regards,
Ross