Part Number: BQ25892
Other Parts Discussed in Thread: BQ25890,
1. The ILIM resistor can be used to set the input current limit for BQ25890/25892. If PSEL is pulled low for BQ25892, will the register setting IINLIM be set as 3.25A by default ? And will this enable whatever the ILIM resistor is used, to control the input current limit ?
2. How to use BQ25892 as 5A charger in standalone mode as the default ICHG is set as 2048mA ? Will writing 5A into the register once, enable it to be used as 5A charger even if the battery is removed and inserted back again ?