Dears,
I am currently using the BQ24196 for charge and discharge management in my device. The registers I set are as follows, REG00=0X37; REG01=0X1E; REG02=0X49; REG03=0X11; REG04=0XC3; REG05=0X88;
At present, 6 boards with BQ24196 have been tested, and the Charge termination voltage(battery voltage) is 4.099V, 4.194V, 4.175V, 3.97V, 3.973V, 3.975V. I think this output voltage deviation is large, which has affected my subsequent power calculation. What do you think of this result?