Other Parts Discussed in Thread: BQ27541
I am trying to write some code to program a bqfs/dffs file into the bq27541 v200 using C over the I2C bus. I am having problems with the "C" command (read and compare): what I read from the gas gauge is not what is expected in the bqfs line. I followed the instructions in the slua541a and I enter the ROM mode first, then as the bqfs/dffs files instructs, my code talks to the I2C address of 0x16. So far I can enter and exit ROM mode successfully, and the "W" command appears to be working.
My questions are:
1) Is there some C example code for programming the bqfs/dffs files into the gas gauge? I have to write a custom program since we are not using the TI EVSW/EV2300 in production.
2) If I don't want to change the GG firmware version, do I still have to program both the bqfs and the dffs or just the dffs will do?
Thank you.