Other Parts Discussed in Thread: BQ78350-R1, BQ78350, BQSTUDIO, BQ76940EVM
I just updated our BMS design to use the new BQ78350-R1 and I am running into calibration problems that I had not experienced when using the previous version of the IC. I am calibrating using the tools available in BQ studio and the error I receive when I attempt calibration of any parameter is as follows: Raw calibration block size returned after command 0xF081 or 0XF082 in an incorrect length.
I have updated my version of BQ studio to 1.3.45 and I have also installed the correct version of firmware into the BQ78350-R1. I did not have problems calibrating before I moved to the updated IC and am curious if the process is different or if I am just missing something obvious.
Thanks
Mike Groft