I'm using a bq40z60 in a custom circuit based on the EVM design. When the charger is disabled, the voltage applied to VAC is reflected accurately in the AC adapter voltage register (after calibration). However, when the charger is enabled, the voltage across the 10k resistor (R14 in the EVM) drops by about 4.7V, from 16.3 to under 12v.
I haven't been able to find a specification for current drain on the 40z60 ACP pin. Can anyone shed light on this?
Should the ACP input resistor (EVM R14) be a lower value?
Thanks.