Hi All,
I'm using the BQ27426 in my new design. To understand what parameters i need to change i connected my BQ27426 to TI battery management studio.
Im using a li-po 110mAh 3.7V battery. i have a few questions:
1. As i understand from the data sheets ( and maybe im wrong) the critical parameter are:
1.chemistry -( i set it to 1202)
2. design capacity - i set it to 110mAh
3. termination voltage - 3400mV
Do i need to change more parameters to get a SOC ?
2. Does the BQ27426 preform a learning cycle automatically or i need to sand a command?
3. i have a strange problem after one cycle (charge-discharge) my SOC dosent updated. any one know what can cuse this problem?
4. im working with a micro controller a a master in my system, each time i turn off my system and on again i need to write the parameters(chemistry , design capacity etc.) to the BQ27426 ? does the BQ27426 save his learning data or i need to save something in the micro controller memory before turning off my system?
thanks for the help