I am having an unusual issue where the fields 'Charging Current' and 'Charging Voltage' remain at zero when charging and only gain a value during discharging.
This is causing the charge to terminate earlier than i would like it to as two of the three conditions are met at all times leaving only one condition controlling the termination.
Is there something that I need to be setting to prevent this happening, I have TCA Set % = -1 to disable that functionality but that seem to be having no effect?
Thanks in advance,
David