It seems that all the registers I need to adjust are read only. Are there any registers that I can adjust to calibrate this chip to my battery? The only one I have been able to adjust so far is the Design Capacity. Other values like the Design Energy, Terminate Voltage, and Taper Rate are mentioned as parameters that are adjusted, but it doesn't mention how to change them.
Alternatively, if I can just upload the parameters set in one board onto many others that would also solve this. I am running a set of batteries through a discharge cycle to train the board to calibrate the right parameters. How would I move those parameters from one board to another?