Goodmorning,
we are developing a new medical handheld device used in surgery.
The device is powered with a primary battery 3V Li/MnO2 like ENERGIZER 123.
Our goal is to prevent the use of the device if the battery SOH il less than 25-30% in order to avoid that the instrument battery dicharges before the end of surgery.
I bought the bq35100 EVM and I'm using it in STATE-OF-HEALTH mode.
The problem is when I replace battery with one not fully charged (due to a battery failure or battery reuse) and I send the NEW_BATTERY command, it assumes that the battery is 100% so the battery heath estimation is wrong.
Which kind of gauge I can use in my application to avoid this problem?
Is possible to estimate the absolute SOH of a primary battery?
Thank you in advance for the cooperation.
Best regards.
Christian.