Hi TI guys:
my Battery is1S2P use the BQ28Z610
bat=4900mAh/P Full bat. V=4300mV
how to set the cWh?
Design Capacity cWh: ??
can you explain: what's cWh ?
thx.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Onyx:
thanks for your reply.
now I give you an example, would you please confirm that the cWh setting is corrert? thx
There are two parallel batteries, each bat.=4900 mAh, bat.v=3700mV. full bat.v=4300mV. follow your answers, the cWH will should be set 4.9*2*3.7/100=0.3626.Is this setting right? thx
add the another question
in the bq28z610 Technical Reference: 13.6.4 Design
default set as below:
Capacity mAh: 4400 mAh
Capacity cWh: 6336 cwh
Design Voltage: 7200 mV
the equation should be as below:
6336=4.4*7.2*200