Part Number: BQ40Z50-R1
First the PEC is off. My SBS Config. register reads: 0x20.
On the documentation, it says that in order to write/read ManufacturerBlockAccess() block 0x44,
the format is : [0x44][cmd][cmd] then read back 2 bytes from register 0x44.
But from looking at the scope, what I saw is there is an extra command: [0x02] in front of the actual command.
For example, trying to read Chem ID, the command is 0006. Based on documentation, the SMB stream should be: 0x44, 0x06, 0x00.
But actually there is a 0x02 right after 0x44. So the actual command send should BE: 0x44, 0x02, 0x06, 0x00.
What I don't know is that where does the 0x02 come from and do I need it for ALL THE BLOCK ACCESS commands?
When reading back, I found out that I have to read back 5 bytes and not 4bytes, I would discard the first byte and read
the last four bytes only. For example, for CHem ID, what I read back is 0x04, 0x06, 0x00, 0x21, 0x01. I have the PEC
turned off I am not sure why I see 0x04 there.
Also the 0x04 is different depends on what is being read back.
Could you confirm this?
Thanks.