Other Parts Discussed in Thread: BQ34110, BQSTUDIO
Hi,
I am working with bq34110 for NiMh multi cell battery, I am using ev2300. I successful calibrated the voltage current and temperature using bqstudio.
I am trying to create the log files required. I am trying to create the log files using the bqstudio.
I clicked into the gpc cycle automated mode
They ask to enter the termination voltage EDVo
Then I can see six different flow diagrams
for eg
low temperature low rate
start- charge-relax-discharge-end
I have fully charged my battery then
I have connected the battery in bat+ and bat- of my board
connected the load in bat+ and pack-
I am a bit not sure about the next step...
start_charge ..am I supposed to do this while charging the battery..
or am i supposed to do this with a fully charged battery.
If I can get some guidance with the set up to create log file it will be very helpful.