Other Parts Discussed in Thread: BQEVSW, BQ27510, BQ27500, GPCCHEM
Hello,
I am working with the 27500-V130 EVM and trying to create a golden image for a new cell we are using. I have been trying to run the learn cycle over the last couple weeks and have two issues, which are probably linked.
1). Any attempt I make at initializing impedance tracking does not seem to work. When I click the initialize button as part of the 4 step learn procedure, the control register never updates to 0021. However, VOK and QEN get set. Control always shows 000B or 000C or other values that i have no idea what they are [NOT 0021]. If I try to manually write 0021 to the flash, when I click enter it just reverts to whatever the value was.
2). Update Status 0 never changes after discharge, charge and discharge ultimately leading to failure of creating golden image.
Some information regarding my set up:
- The cell I have is a 305mAH Li/NCA cell, and customer provided "closest chemistry is 210". So I chose the 0210 chemistry. That is all i know about cell.
- I selected internal temp sensor and have an 8.2K resistor connected between BI/OUT and PACK -. BAT_DET register is set (wasn't previously setting until I connected external resistor)
- All my configurations have been set up [4.1V charge, 305mAH capacity, constant power output etc...]
- Registers seem to be showing proper operation, which is confusing me more on why IT_ENABLE and UPDATE STATUS 0 are not working. CHG and DSG set during charge and discharge, VOK and QEN get set before charging and after I click the "initialize IT" button and fuel gauge on bottom left goes from 0-100 when charging and from 100-0 when discharging [how accurate it is I dont know].
Lastly, I am not following the 2hrs after charge and 5 hrs after discharge, these times are much longer. I have followed same timing on all my attempts:
1). Start with fully charged and relaxed battery. Discharge down to 3V with C/5. [rather than 5hrs, system sits overnight]
2). Next morning click "Dsg/Wait Done" and "Initialize IT" and charge to full 4.2V with C/2 and click "Charge/Wait Done" after 2 hrs so FC bit doesn't clear. Then system sits overnight.
3). Next morning begin discharge to 3V with C/5. At this point, I can see UPDATE STATUS is still 0. As far as I have gotten.
Any ideas on something/things that I am doing wrong?
Mike