This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: exiting shutdown mode of the BQ40Z50 using the LED display button

Part Number: BQ40Z50
Other Parts Discussed in Thread: , TIDA-00883

The BQ40Z50 supports a very low quiescent current time-based shutdown mode, which is great for increasing shelf life of a battery.

Here's some info from the technical reference manual

*******

The bq40z50-R2 device can be configured to shut down after staying in SLEEP mode without communication for a preset time interval specified in Auto ShipTime.

Setting the PowerConfig[AUTO_SHIP_EN] = 1 enables this feature.

Any communication to the device restarts the timer.  When the timer reaches Auto Ship Time , the time-based shutdown effectively triggers the MAC shutdown
command to start the shutdown sequence.

The bq40z50-R2 device returns to NORMAL mode when voltage at PACK pin > VSTARTUP

*******

I would like timed shutdown to be exited on a removable battery when the LED charge status display push-button is pressed. 

This would allow checking charge status on a timed shutdown pack without requiring the pack to have a voltage applied externally to wake up the pack.

Looking at the schematic for the TI reference design at tida-00883, it appears there is an opportunity to use the LED pushbutton to turn on a P-MOSFET that would connect the BAT pin, through a 10K resistor + isolation diode to the PACK pin when the LED display pushbutton is pressed.  This would allow "local wakeup" of a battery pack without the need for an external voltage to be applied.  This would be valuable when checking the actual charge status of a battery that had entered timed shutdown.

One problem with this approach is finding a P-MOSFET with a low enough off state leakage current.  For example, the BSS84 has a 15ua off state max leakage, which would not be good enough for the 2 meg ohm input impedance PACK pin of the BQ40Z50.

Any ideas on how to make the BQ40Z50 wake up from timed shutdown with the LED display button?