Hi Ti experts,
I want read bq28z610 cell 1 voltage &cell 2 voltage by MCU, but no the command about them in BQ28Z610 TRM.
Could you help to provide the command of read bq28z610 cell 1 voltage &cell 2 voltage ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti experts,
I want read bq28z610 cell 1 voltage &cell 2 voltage by MCU, but no the command about them in BQ28Z610 TRM.
Could you help to provide the command of read bq28z610 cell 1 voltage &cell 2 voltage ?
Thanks
Batt said:Hi Ke,
It's simple. Just write 0x7100 to register 0x3e. Then read 36 bytes from it. The second and third bytes in it will give you cell voltages 1 and 2 in little endian.
eg. on my gauge writing 0x7100 to 0x3e gives 71 00 EC 0F F7 0F 00 00 00 00 D1 1F 8D 1E 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 F2 24 where, EC 0F and 0F F7 are cell 1 and cell 2 voltages.