Hi,
I was going through some of your documents on impedance tracking. I wanted to understand how it works so that I can shift to Impedance track from CEDV gauge that I have.
This is my understanding:
Qmax is the full capacity that is first learned by calculating Passed Charge/(SOC1 - SOC2). During current discharge, coulomb counting is used to update the SOC. At some specific points of DOD, resistance update takes place and you store it in a lookup table. After that,
Full charge capacity is updated, Full Charge Capacity = Qstart + Passed Charge + Remaining Capacity. The Remaining Capacity is estimated by a simulation which decreases the DOD till the termination voltage is reached.
I have following doubts now:
1. Is Qmax same as Full Charge Capacity? Do we keep updating Qmax = Passed Charge/(DOD1 - DOD2) during 2 relaxed states during the normal running application? OR Full charge capacity takes care of the new capacity of the battery as the battery ages? Basically, I am confused between Qmax and FCC (full charge capacity). Are FCC and Qmax same at the start and how do they update during the normal run?
2. Does internal impedance play a role only for measuring the remaining capacity RM? How does it take into account the SOH? I am unable to understand it intuitively. I understand that internal impedance will increase with aging but how are we using this fact?
3. How many resistance measurements do you have in the look-up table? Do you interpolate the rest of them?
4. What is the difference between:
DataRAM.Full Charge Capacity( ) and DataRAM.Full Available Capacity( ) and DataRAM.Nominal Avail. Capacity( )
5. Does not the OCV voltage also change with aging of batteries?