i AM USING A YUASA PbA NP7 12V BATTERY WITH A CONSTANT POWER LOAD. FURTHERMORE I AM USING THE BATTERY MANAGEMENT STUDIO WITH THE BQ34Z110 CHIP. IN ORDER TO MAKE MORE EEFICIENT MY PRODUCT THERE IS A SORT OF QUESTION OR DOUBT I WOULD LIKE TO UNDERSTAND REALLY WELL.
WHAT I WOULD LIKE TO KNOW HOW TO PROPERLY CONFIGURE THE BIT FC SET %. LEAVING THIS PARAMETER BY ITS DEFAULT VALUE OF 100 I NORMALLY REACHED TO SET THE FC BIT. IN THE SAME WAY, CHANGING THIS FC SET% PARAMETER TO -1 , IT TAKES MORE TIME TO TRIGGER THE BIT FC SETS DUE TO THE TAPER CURRENT THAT SHOULD BE BIGGER THAT THE BATTERY CURRENT. IN BOTH WAYS, THE BIT FC SETS TO 1, BUT I WOULD LIKE TO KNOW WHICH OF TWO CONFIGURATIONS WOULD BE BETTER FOR MY APPLICATION.