Dear My friends
I am trying to programming my UCD9240 control board using TI fusion GUI for 200V normal operation Vin buck converter and 48V output voltage, however I met one cirtical problem on input voltage configuration. Acturally, from GUI desinger, the input voltage can be defined up to maximal 400V according to the recommendation. In GUI configuration, the Vin warn limit and Vin Fault limit is only allowed to be defined lower than 24V. I can not 100% make sure if UCD9240 really can be applied for this high voltage application. According to my regarding, I think I can use resister divider net to provide required input votlage range, such as deviding 200VDC input to 20VDC and then using another resistor divider net as voltage scaling to configure the required input votlage for hardware. It means I have to lie to GUI software for system configuration. Meanwhile for the output voltage I would like to employ the same resistor divider net.Therefore here I would like to ask friends and TI engineer if I can make such kind of supporting in order to have the same operation condition for high input voltage buck converter???
Thanks for answer and help from friends and TI engineer in advance.
Jack