Other Parts Discussed in Thread: UCD9244
Dear Ti
I use Fusion Digital Power Designer 2.0.40
I have a PCB with UCD9244 device on. The design has already been verified.
One board gives the following problem:
When I run the Fusion tool, it detects one device, but when the GUI tries to open, it gives the following error =>
Cannot read VOUT_MODE(see message at bottom).
When I run the I2C / SAA debug tool, I can read the VOUT_MODE as 0x14.
I tried to run the UCD Debug tool, but it requires a password.
Please provide me with the password.
Is there a way to enable the Fusion GUI in order to erase the UCD EEPROM ?
Please advise
Kind regards
Piet
There was an error bootstrapping the Fusion GUI for the UCD9244 @ Address 18d:
The following PMBus commands could not be read from the UCD9244 @ Address 18d:VOUT_MODEThese commands are required for Fusion Digital Power Designer to run.Please verify firmware and power and try again or contact customer support if you continue to have difficulties. at TIDP.PMBus.ad.a(PMBusDevice A_0, IEnumerable`1 A_1) at TIDP.WinForms.Apps.DPGUI.jl.oe() at TIDP.WinForms.Apps.DPGUI.jl.ok()
The Fusion GUI can not continue due to this error.