Other Parts Discussed in Thread: UCD9244, UCD74120
I use these two chips to generate a freescale T2080 VDD power.
Input voltage is 12V and ouput voltage is 1.025V.
When the switching frequency is above 1000khz,sometimes there will be no ouput voltage and FLT bit will be set in GUI.
It is all right when the switching frequency is below 1000khz.
Why?
Here is my schematic and project file.
I only change the switching frequency to 1100khz and there will be some failure.