Hello.
Might I ask what resistors power ratings are required for shunt regulator in Fig. 27 of the datasheet?
The power amp board I'm using TL431 which is set for 15V out has some oscillation at a start, so called "motorboating". Could the source of instability be TL431 if maximum current out reached? To suppress this instability should I use 0.22uF between cathode and anode?
The maximum current for TL431 at 15V out is only 20mA?
Thanks,
Andriy.