Other Parts Discussed in Thread: BQ24210, BQ25570
Hi All
I need to charge a 2000mAh 4.2V Li-poly battery using a very small solar panel. My solar panel is Rated at 5V 250mA. Currently I have connected the solar panel via a load switch(TPS27081ADDCR ) to the battery and using the ADC from a micro controller I check the voltage of the battery to avoid over charging the battery and that once the battery reaches about 4V(full charge) the charging stops by disabling the load switch. I have avoided using a Li-charger IC for this solar application simply because the power rating of solar panel is low and many IC's require a minimum voltage and current, this way even if the solar produces low power due to a low sun , the battery will get some charge compared to nothing with an IC.
Would you be able to suggest any better method or if a new charging ic is available, keeping in mind that solar panel used will be of low power?
Regards
DJ