Hi,
May I check if TI has EMI performance data for LMR14030? (i.e is LMR14030-Q1 meets CISPR 25 standard?)
I can only locate some EMI related information for LM4360x and LM4600x (applicatio note) but couldn’t find any info on LMR14030-Q1
Below is the LT8614 (LTC DCDC) EMI performance below for your reference.
In LT8614 D/S, there are Radiated EMI Performance data for the following condition.
14VIN TO 5VOUT AT 4A, fSW = 2MHz
So, It'll be very helpful if you can provide us the EMI performance data under similar conditions,
(Like Same VIN, VOUT, fSW and max Iout)
Thanks