Part Number: TL431
Hello.
I used TL431.
This Circuit.
What is the voltage at this point?
I don't Konw....
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TL431
Hello.
I used TL431.
This Circuit.
What is the voltage at this point?
I don't Konw....
Thanks.
Thank you for your reply.
The primary side circuit is as follows.
PC817 CTR = Min50%, at If = 5mA
Optocoupler Opaerating State
PC817 Output side Ice = 0.22mA,
Input side = 0.22mA / 0.5(CTR 50%) = 0.44mA
------------------------------
I want cathode voltage.... get a estimated range..
R2.. remove...
Vr1 = 600*0.44mA = 0.264V
optocoupler VF = about 1V
12-1V(Vf) - 0.264V = 10.736V right?
Thanks.
That is correct. I would not remove R2 in your final design, as 440 uA is not enough to properly bias the TL431 in worst case conditions.
Hope this helps,
Ethan