This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5010A: EMI Issue

Part Number: LM5010A

Hello,

My customer is using the LM5010A buck converter, 48Vdc to 3.3Vdc.  The 48Vdc VIN is also used for Power over Ethernet out RJ45 port.  The board fails EN55032 Telco Conducted emissions tests at the 1.8MHz, the same frequency as the switching rate of the LM5010A. In order to pass the emissions test the noise from VIN needs to be removed.  The customer is providing schematic and layout which I can PM.

Thank you for your support!

Errol Leon

Texas Instruments

Field Applications Engineer