Other Parts Discussed in Thread: PMP6812
Dears:
Pls. refer the before post, the customer has debugged the board and have an issue.
12V output, the load power consumption exceeds 21W will burn MOS; when 20W, MOS will be very hot, it will burn out after a long time.
1. What should be the normal level of GATE?
2, Kindly help to look at the diagram, the current maximum frequency of transformer support is 200K, FRS resistance is 69.8K, the switching frequency is about 250K, is it OK?