I'm adding voltage regulators (2 x LM338) to an existing power supply that powers a 12A rms current source. Regulating from +/-36Vdc down to +/-30Vdc. The original supply only produces +/- 3Adc however the current source is used intermittently for very short bursts (< 16ms), so I will rely on very large bulk capacitors to supply the required current for the short burst. I'm inclined to put the bulk capacitors on the output for the following reasons:
- 35V vs 50V capacitors
- Peak surge current does not have to flow through the regulator (data sheet states 12A for 0.5ms)
I will rely on the internal current limit to protect the device on power-up (charging the big caps).
Any reason not to take this approach?