Other Parts Discussed in Thread: TIDA-01573
Hello support team,
My customer would like to understand equation(1) in the TIDA-01573.
http://www.tij.co.jp/jp/lit/ug/tidue52/tidue52.pdf
In p.4, equation (1) : 60A*1ns/2V = 30nF capacitance
In this case, 2V means 5% of Vbus 40V. Is this right?
If so, worst case voltage across a laser diode is 38V.
Should not 38V be used for the capacior calculation instead of 2V?
Best regards,
Kaizawa