Part Number: LMG3410
Hello,
I have two of the LMG3410 implemented in an inverting buck-boost converter. One of them works as a switch. The other one replaces the diode so that the source is connected to the load and the output capacitor. So a part of the time (depending on the Duty-Cycle) the transistor has a voltage drop of Ui+Uo over it and the other time it conducts current from source to drain so it should work as given in figure 3 of the datasheet.
The maximum input voltage of the converter should be 150V. When I test the converter with an input of for example 30 V and in boost mode with Uo=1,5*Ui everything works fine. That means when the Transistor conducts current the Voltage drop is about -7V. When I increase the Input Voltage also everything works as it should up to when the voltage drop over the transistor which works as a diode reaches about 200V (80V input, 120V output). If I increase the input voltage now the voltage drop over the transistor changes from about -7V proportional towards 0V and even higher to a positive value. Just before that happens the lower falling edge of Ugs gets rounded and the curve of Uds gets crooked somehow and then the whole curve gets raised. After a short time the LMG3410 shuts off.
To increase or lower the current through the device changes nothing.
The other Transistor works as it should. The external wiring of both tansistors is identical. For the layout I used an example layout of TI.
I tried to control the diode-transistor with a PWM and to ground the input pin, but nothing changes, in both cases Uds=-7V and the error occurs. I thougt if I drive the device with a PWM the Uds should be nearly 0V even in 3. Quadrant, but it isn't. Isn't the device capable to be driven in 3. Quadrant easily?
So I hope you understand my problem and can help me to fix it.
Best regards,
Colin Setzke