Hi everybody!
We're currently designing a Full Bridge ZVS 3400W converter with two UCC28950 (coupled as master/slave interleaving).
For current sensing we're using the Si8503 (recommended by a TI employee in another post). The output of the Si8503 is amplified in order to match the input of the CS on the UCC28950. The Si8503 should be a much better choice than a common current sense transformer due to it's leading edge blanking.
We're concidering load sharing using two UCC39002 since the output of the two UCC28950 is only tied together by the two output inductors (the UCC28950 is run from the secondary side of the full bridge transformer).
The output of the Full Bridge converters is 40V and up to 3400W output total.
How should we get this done?
Should the voltage feedback from the output be tied together on the two UCC28950 and only measured from one of the outputs?