Hi,
I am currently doing a project on Regenerative Braking on E-Bike. To control the 24V DC Motor, I have choose the ""60-V, N-Channel NexFET™ Power MOSFETs"" and ""LM5101A/B/C 3A, 2A and 1A High Voltage High-Side and Low-Side Gate Drivers"" as my mosfet gate driver.
I having trouble on choosing the Bootstrap Capacitor values and Diode, and also with the 24V DC motor, is 60V mosfet is okay for my design? I have search some info in the net saying that for 24V DC Motor, 60V mosfet would be recommended.
Extra questions:
I am going to drive the DC Motor using Microcontroller to produce PWM signals. By fed in the PWM signals to the mosfet driver and to drive the power mosfet to control the DC motor speed.
Please help me in this problem. Thanks and any helps is appreciate.
**Note: The name of the devices is taken from the title of the datasheets.