A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC28C40 voltage on pins: is it OK to have 3.3V on the Rt/Ct pin, when there is zero volts on the Vdd pin?
No it is not a good idea to have an input voltage on any of the pins when the Vdd supply is zero. This will likely cause a parasitic turn on within the part and cause a failure. The UCC28C40 has not been characterized for this but it may be acceptable to add a reverse polarity Schottky diode between Rt/Ct and Vdd and this will protect the chip when Vdd is zero.