Other Parts Discussed in Thread: UCC28700, UCC28730, UCC28911
Dear support member,
My customer used UCC28910.
Specification condition
Vin:74V~264V
Vout:12.7V
Iout:0.5A
Primary Vcc:19V
Vcc Current:0mA~51mA
I have two question.
Q1.
When the load of 19 V system changes with 0 mA - 51 mA,
I think that the Vcc voltage also changes a little.
By setting resistance as Pre-Load,
Is it possible to limit the 12 V output accuracy on the secondary side to within ± 7%?
Q2.
Where should the measurement position the Bode plot measurement?
Is it measured with the resistance of the VS pin?
Best regard.
Bob Lee.