Universal Input 85-265Vac to 24Vdc @ 0.4A output.
Everything is working, except when turned on with heavy output load UCC28710 goes into protection mode. If still powered, unplug the load, and plug load back in, output voltage goes back up to 24Vdc, and current back to rated at 0.5 Amps.
So if an end user were to use this, and the power goes out, and comes back on, then they would need to manually go to where ever power supply is installed, and open and close the load.
What would be the best application recommendation on the output so make sure the UCC28710 is up and running, before it powers the output for the heavy load.
Using primary side auxiliary feedback.
I was thinking maybe a voltage detector, but wanted some advice or direction from an applications engineer that may have ran across this before.
Thanks for any feedback, or pointers to another similar question posted as I couldn't find one like my question.