Hi,
I am deciding on the power path management for my new project and wanted to consult TI experts. My new device is going to work from Battery and already has a TI battery management IC - BQ51050BRHLR.
The output of the BQ51050BRHLR is 4.2V and I need to lower it to 3.3V for the whole system. The average current consumption will be around 10 mA - 20mA with 100mA max. peaks. I don't know if an LDO is a good choice since ca. 90 mW will be dissipated in worst case scenario and ca. 15-20mW on average. I was thinking of maybe taking an efficient SW Regulator although I don't know our current consumption in the sleep mode... so this is one problem.
There is also another issue: one IC can jump from 5mA to 60mA very fast, the rest of the circuitry is slow with no high transient peaks. So, I was thinking if I should take one IC with two channels, two ICs or one IC with one channel and just separate paths with caps and maybe ferrite bead.
Any solution suggestion with TI ICs will be appreciated.
Kind Regards,
Den