Hi,
There is OPP, PCL for current protection.
The Vcst(opp) range is 0.425V to 0.6V, and PCL value is set to 0.8V.
Could you help explain what is the difference between OPP and PCL?
If the full power is 65W, and the OPP is 78W. When we put a 130W at the output for 10ms, how is the reaction of the current sense voltage Vcst? 0.8V or OPP threshold?
When it will trigger PCL?
Thanks!
BR
Eleven Chen