In the datasheet, there's only RC recommendation for Vout= 10V , when Vout is 6.2V , what the RC should be? if there's any risk when we choose the same RC value (output voltage = 10V)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the datasheet, there's only RC recommendation for Vout= 10V , when Vout is 6.2V , what the RC should be? if there's any risk when we choose the same RC value (output voltage = 10V)?
Hello April,
Section 9.2.1.2 on page 13 of the data sheet gives out simple formulae for calculating design values. The only values that need to be calculated are R1, R2, R3, R4, C9 and C10. Based on design requirements in the datasheet and VPOS/VNEG set voltages of +/-6.2V, I calculated following values. Please choose the closest standard available component values for your design.
R1=534.4K
R2=130K
R3=619.4K
R4=121.2K
C9=12.7pF
C10=12.1pF
Kind Regards,
Liaqat