Other Parts Discussed in Thread: TLC59711, SN74LS04
Hi,
I want to make a prototype of LED driver with the TLC 59711 but I can't find the output PWM switching frequency in the data sheet. Is it a constant or can I change it?
Many thanks
Yan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, Yan,
59711 use internal grayscale clock, which is 10MHz typical. To finish a complete display period(65536 GCLK cycles) , the PWM frequency should be 152Hz typical, you can't change it.
While, tlc59711 use ES-PWM (128 segments in one display period), thus the measured PWM frequency at output pin will be 152*128=19.5kHz.
The above calculated PWM frequency is correct when GS>128. When GS<128, the output pin turn-on frequency is not constant since some segments have no chance to turn on yet.
Since the internal grayscale clock have some variation(minimum 7MHz, maximum 12MHz), then the PWM frequency will also have variation accordingly.
Best regards
Mike
Hello Mike,
Thanks for your answer, as expected I measured a 20kHz on each output. For my project I need to drive 12 high current output (4>6A Led), so I try to find a interface between the collector output of TLC59711 and power N mosfet. I've try several options, for example a mosfet driver with internal input pull-up (fan3226), a logic inverter with pull-up too (SN74LS04). At very low PWM output (0-3% of duty cycle), the mosfet driver could not perform a smooth start; and the inverter solution is influenced by the level of other outputs (think that's because of the current needed by the gate at 20kHz. Have you an idea to better interface TLC outputs and N mosfets while keeping non-inverting signal?
Thank you and best regard,
Yan