Hello guys,
One of our customers is evaluating LED171596A using the device EVM. They bought the EVM in last month (March) and the EVM worked without any problem with GUI control software and MSP430 launch pad. According to the silk printing on the EVM PCB, the EVM version they boght in March is Rev.E1 and the board color is green.
They bought 3 EVMs of LED171596A as additional this month (April). But all of those EVM didn't work with same GUI control software and launch pad for Rev.E1. All EVMs version are Rev.A and All PCB color are red.
Could you please give me your answer to the following questions?
1. Which version is the official EVM at this moment?
2. Can both versions work correctly with same version of control software and MSP430 launch pad?
3. When the answer for No.2 is No, how they can use the EVM correctly? Do they need another version of control software and lauch pad?
Your answer would be much appreciated.
Best regards,
Kazuya Nakai.