Other Parts Discussed in Thread: LM317, TL783, PTH12040W
A student came to me with a spec from the LM317 datasheet (SLVS044U) and I cannot answer his question. In the Electrical Characteristics table for Maximum Output Current, with Vi - Vo <= 40V, Pd < Pmax, and Tj = 25C, the typical output current is 0.4A. I'm confused as to this spec. Does the maximum output current really drop when the differential voltage across the device exceeds 15V? I have always assumed that as long as I provide sufficient heatsinking to keep the junction temperature below the maximum (preferably well below) and do not exceed the max input voltage, the regulator will provide up to the max output current. The inclusion of Tj = 25C is confusing as well as it's unlikely the junction temperature would be at room temperature for all but the lightest of loads.
The student pointed out the TL783 data sheet which has a similar reduction in peak output current, but the spec includes a time parameter as does the graph on page 4 of that TL783 data sheet. Is this spec a pulsed current limit?
Could you shed some light on this for us. The students in the Electronics Club are designing some high output current supplies for use in 3D printing and also some high voltage applications.