Sorry to bother.
application condition as below.
Vin=20V, SHDN pin=0V, Out pin can measure 2.45V
Vin=15V, SHDN pin=0V, Out pin can measure 1.45V
is it correct??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There are a few things that I can think of that may cause the output of an LDO to be above 0V when disabled:
-Kyle