Hello,
My customer wants to set "Vo: 1 V, Io: 0.959 A" at "Vin: 1.5 V, Vbias: 3.3 V, Ta: 0 to 60 ° C." using TPS74801.
In order to know the lower limit value of Vin, please tell me the value of "Vdo" under the above conditions.
I would appreciate it if you can get graphs of (Vbias - Vo) versus Vdo when Io is 1A.
Thank you.