Hello,
we are using the LP2985 in a board which we produce now a few years, and everthing was fine.
Now the last boards have problems, and I pinned it down to the LDO.
It seems the last LDOs we used have dropout voltage that is too high.
For testing purpose I assembled the LDO on an extra board and used a resistor to draw current.
(Cin = 4µ7-X5R / Cby = 10nF-X7R / Cout = 2µ2-X7R / LP2985IM5-3V3 / R-load = 47R / load = 70mA)
The old LDO held the output to 3,27V when changing the input voltage from 4V to 3.4V
The new LDO can't hold the output voltage // 4V = 3.15V / 3.8V = 2.99V / 3.6V = 2.82V / 3.4V = 2.65V
I checked the printings on the parts and both have "L0RB", the only difference is the marking on the old one is looking bolder than the marking on the new one.
So I'm not really sure, this is ok for the device, or is there a possibility that i got counterfeid parts?
Thank you
Stefan