This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS737: Load Regulation performance

Part Number: TPS737

I am applying TPS73701 (Adjustable OUT, Set to 3.3V) to my application.

When I checked load regulation of it, result show marginal failure when I apply 0.0005%/mA criteria.

Can you review the test condition and result if the result is valid or not?

Test set-up.

Apply actual use case instead of electric load. 

Condition : 90mA<IOUT<783mA

Criteria : 0.005%/mA applied to judge Pass/Fail

Calculation : Referred to Iout=90mA and Vout@90mA 

Result

Iout(mA) ΔIOUT Vout ΔVOUT ΔVOUT(ΔIOUT) %
90 0 3.29 0 0
230 140 3.288 0.002 0.0004
270 180 3.284 0.006 0.0010
318 228 3.286 0.004 0.0005
374 284 3.286 0.004 0.0004
413 323 3.284 0.006 0.0006
430 340 3.284 0.006 0.0005
464 374 3.284 0.006 0.0005
604 514 3.282 0.008 0.0005
633 543 3.277 0.013 0.0007
672 582 3.276 0.014 0.0007
717 627 3.28 0.01 0.0005
755 665 3.279 0.011 0.0005
783 693 3.278 0.012 0.0005